AXIS#.WS.DISTMIN

Description

This parameter sets the minimum movement that is required for commutation finding. If this value is too small, then the commutation finding might fail if too little current is used. The larger this value, the more movement is needed in order to avoid F5500: "Wake and Shake - Insufficient movement".

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Actual position units

Range

0 to 90 deg

Default Value

1 deg

Data Type

Float
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
AXIS1.WS.DISTMIN

5013h

0fh

Signed32

Position

-

Read/Write

No

AXIS2.WS.DISTMIN

5113h

0fh

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.DISTMIN

6702

1A2E

Signed32

Read/Write

Position

AXIS2.WS.DISTMIN

72238

11A2

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.DISTMIN

6702

Signed32

Read/Write

Position